Normal voltage range for VDD_LV 1.2v Core Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Normal voltage range for VDD_LV 1.2v Core Voltage

Jump to solution
1,922 Views
john_floros
NXP Employee
NXP Employee

Hello,

Nominally the Core Voltage (VDD_LV) for the S32K1 is 1.2v.  This can be measured using the ADC.  What would be the valid range for the core voltage if a customer wanted to verify that the voltage was good?

0 Kudos
Reply
1 Solution
1,907 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi John,

the core voltage is generated internally, it can’t be affected by user. Therefore, it’s not specified in the datasheet. The voltage is monitored by low voltage detector which generates reset if it is outside of the thresholds. See LVRFLG register in the reference manual.
If the core voltage is OK (as well as all other supply rails) then the device is up and running. If the core voltage gets out of that range, the microcontroller is reset.
So, checking of core voltage by ADC is meaningless and there’s no reason to specify the values in the datasheet.

Regards,
Lukas

 

View solution in original post

0 Kudos
Reply
1 Reply
1,908 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi John,

the core voltage is generated internally, it can’t be affected by user. Therefore, it’s not specified in the datasheet. The voltage is monitored by low voltage detector which generates reset if it is outside of the thresholds. See LVRFLG register in the reference manual.
If the core voltage is OK (as well as all other supply rails) then the device is up and running. If the core voltage gets out of that range, the microcontroller is reset.
So, checking of core voltage by ADC is meaningless and there’s no reason to specify the values in the datasheet.

Regards,
Lukas

 

0 Kudos
Reply