Normal voltage range for VDD_LV 1.2v Core Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Normal voltage range for VDD_LV 1.2v Core Voltage

ソリューションへジャンプ
1,432件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

Nominally the Core Voltage (VDD_LV) for the S32K1 is 1.2v.  This can be measured using the ADC.  What would be the valid range for the core voltage if a customer wanted to verify that the voltage was good?

0 件の賞賛
返信
1 解決策
1,417件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi John,

the core voltage is generated internally, it can’t be affected by user. Therefore, it’s not specified in the datasheet. The voltage is monitored by low voltage detector which generates reset if it is outside of the thresholds. See LVRFLG register in the reference manual.
If the core voltage is OK (as well as all other supply rails) then the device is up and running. If the core voltage gets out of that range, the microcontroller is reset.
So, checking of core voltage by ADC is meaningless and there’s no reason to specify the values in the datasheet.

Regards,
Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,418件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi John,

the core voltage is generated internally, it can’t be affected by user. Therefore, it’s not specified in the datasheet. The voltage is monitored by low voltage detector which generates reset if it is outside of the thresholds. See LVRFLG register in the reference manual.
If the core voltage is OK (as well as all other supply rails) then the device is up and running. If the core voltage gets out of that range, the microcontroller is reset.
So, checking of core voltage by ADC is meaningless and there’s no reason to specify the values in the datasheet.

Regards,
Lukas

 

0 件の賞賛
返信