No power on S32K144 and it really gets hot when powered through 12V or USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No power on S32K144 and it really gets hot when powered through 12V or USB

559 Views
josephcoorey
Contributor I

Hi, I am working with a S32K144. I plugged in the board yesterday into 12V, and saw some blinking in the reset light. Now I don't have power to the board. When I plugged into USB without power, I see 1 green LED. When I enable power through 12V or USB, the board gets really hot. 

Any help would be appreciated. 

Thanks!

0 Kudos
1 Reply

535 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @josephcoorey,

Which chip is heating on the board?

I reckon it is the S32K144 MCU since it gets hot regardless of the power source.

I'm afraid the MCU has been damaged.

 

BR, Daniel

 

 

0 Kudos