Need information regarding MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need information regarding MCU

494 Views
pratayay123
Contributor III

what is the operating voltage of the input ADC pin ..0-3.3 volt or 0-5 volt?

0 Kudos
1 Reply

489 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you did not specify the MCU, lets assume S32K144.
ADC input should be between VREFL and VREFH. Recommended condition is to have VDD=VDDA=VREFH. Anyway VDDA and VDD must be shorted on PCB, but VREFH can be connected to another source. And there is a restriction, VREFH should be equal or less than VDDA + 0.1V and VDD + 0.1V.

BR, Petr

0 Kudos