Hi,
I am trying to flash a S32K344 MCU (specifically, on the MR-CANHUBK344 board) with PyOCD. Mostly, I am trying to get it to work with MCU-Link. However, flashing does not work with MCU-Link or J-Link.
I've confirmed that flashing works with J-Link when I use Segger's software, so my hardware setup is good.
I pasted the error that I get after running `pyocd load -t s32k344 -O connect_mode=reset-and-halt <path_to_my_hex> -vv` at the bottom of this post. I get this same error with MCU-Link or J-Link. Resetting the core seems to work, FWIW.
Can someone tell me what I am doing wrong, or can suggest how I can continue debugging this? I am using pyocd 0.42.0
Any helps, tips, or points in the right direction is very appreciated. Thanks in advance!
```
0000246 I Target type is s32k344 [board]
0000258 D Running task load_svd [sequencer]
0000258 D Running task pre_connect [sequencer]
0000258 D Running task dp_init [sequencer]
0000258 D Running task lock_probe [sequencer]
0000258 D Running task get_probe_capabilities [sequencer]
0000258 D Running task connect [sequencer]
0000260 D Default wire protocol selected; using SWD [dap]
0000261 I DP IDR = 0x6ba02477 (v2 rev6) [dap]
0000261 D Running task clear_sticky_err [sequencer]
0000261 D Running task power_up_debug [sequencer]
0000261 D Running task check_version [sequencer]
0000261 D Running task unlock_probe [sequencer]
0000261 D Running task unlock_device [sequencer]
0000261 D Running task create_discoverer [sequencer]
0000261 D Running task discovery [sequencer]
0000261 D Running task find_aps [sequencer]
0000262 D Running task create_aps [sequencer]
0000262 D Running task create_ap.1 [sequencer]
0000264 D APB-AP#1 default HPROT=0 HNONSEC=0 [ap]
0000264 D APB-AP#1 implemented HPROT=0 HNONSEC=0 [ap]
0000265 I APB-AP#1 IDR = 0x54770002 (APB-AP var0 rev5) [discovery]
0000265 D Running task create_ap.4 [sequencer]
0000266 D AHB-AP#4 default HPROT=b HNONSEC=0 [ap]
0000267 D AHB-AP#4 implemented HPROT=f HNONSEC=1 [ap]
0000267 I AHB-AP#4 IDR = 0x84770001 (AHB-AP var0 rev8) [discovery]
0000267 D Running task create_ap.6 [sequencer]
0000268 I AP#6 IDR = 0x001c0030 (AP var3 rev0) [discovery]
0000268 D Running task create_ap.7 [sequencer]
0000268 I AP#7 IDR = 0x001c0040 (AP var4 rev0) [discovery]
0000268 D Running task enable_debug [sequencer]
0000268 D Running task find_components [sequencer]
0000268 D Running task init_ap.1 [sequencer]
0000271 I APB-AP#1 Class 0x1 ROM table #0 @ 0x80000000 (designer=00e:NXP part=995) [rom_table]
0000277 I [0]<80001000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0> [rom_table]
0000281 I [1]<80002000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0> [rom_table]
0000284 I [2]<80003000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0> [rom_table]
0000288 I [3]<80004000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0> [rom_table]
0000292 I [4]<80005000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=480:0:0> [rom_table]
0000295 I [5]<80006000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0> [rom_table]
0000299 I [6]<80007000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0> [rom_table]
0000303 I [7]<80008000:HTM CS-400 class=9 designer=43b:Arm part=917 devtype=43 archid=0000 devid=0:0:0> [rom_table]
0000306 I [8]<80009000:CTI CS-400 class=9 designer=43b:Arm part=906 devtype=14 archid=0000 devid=40800:0:0> [rom_table]
0000312 I [9]<8000a000:TPIU CS-400 class=9 designer=43b:Arm part=912 devtype=11 archid=0000 devid=a0:0:0> [rom_table]
0000315 I [10]<8000b000:SWO CS-400 class=9 designer=43b:Arm part=914 devtype=11 archid=0000 devid=ea0:0:0> [rom_table]
0000318 I [11]<8000c000:TSGEN class=15 designer=43b:Arm part=101> [rom_table]
0000318 D [12]<0000d002 not present> [rom_table]
0000318 D [13]<0000e002 not present> [rom_table]
0000318 D [14]<0000f002 not present> [rom_table]
0000318 D [15]<00010002 not present> [rom_table]
0000318 D [16]<00011002 not present> [rom_table]
0000318 D [17]<00012002 not present> [rom_table]
0000320 D [18]<00013002 not present> [rom_table]
0000320 D [19]<00014002 not present> [rom_table]
0000320 D [20]<00015002 not present> [rom_table]
0000320 D [21]<00016002 not present> [rom_table]
0000320 D [22]<00017002 not present> [rom_table]
0000320 D [23]<00018002 not present> [rom_table]
0000320 D [24]<00019002 not present> [rom_table]
0000320 D [25]<0001a002 not present> [rom_table]
0000320 D [26]<0001b002 not present> [rom_table]
0000322 D [27]<0001c002 not present> [rom_table]
0000322 D [28]<0001d002 not present> [rom_table]
0000322 D [29]<0001e002 not present> [rom_table]
0000322 D [30]<0001f002 not present> [rom_table]
0000322 D [31]<00020002 not present> [rom_table]
0000322 D Running task init_ap.4 [sequencer]
0000326 I AHB-AP#4 Class 0x1 ROM table #0 @ 0xe00fe000 (designer=43b:Arm part=4c8) [rom_table]
0000330 I [0]<e00ff000:ROM class=1 designer=43b:Arm part=4c7> [rom_table]
0000330 I AHB-AP#4 Class 0x1 ROM table #1 @ 0xe00ff000 (designer=43b:Arm part=4c7) [rom_table]
0000335 I [0]<e000e000:SCS v7-M class=14 designer=43b:Arm part=00c> [rom_table]
0000337 I [1]<e0001000:DWT v7-M class=14 designer=43b:Arm part=002> [rom_table]
0000340 I [2]<e0002000:FPB v7-M class=14 designer=43b:Arm part=00e> [rom_table]
0000342 I [3]<e0000000:ITM v7-M class=14 designer=43b:Arm part=001> [rom_table]
0000342 D [4]<fff41002 not present> [rom_table]
0000342 D [5]<fff42002 not present> [rom_table]
0000346 I [1]<e0041000:ETM M7 class=9 designer=43b:Arm part=975 devtype=13 archid=4a13 devid=0:0:0> [rom_table]
0000349 I [2]<e0042000:CTI CS-400 class=9 designer=43b:Arm part=906 devtype=14 archid=0000 devid=40800:0:0> [rom_table]
0000349 D [3]<1ff02002 not present> [rom_table]
0000349 D Running task create_cores [sequencer]
0000349 D Creating SCS component [discovery]
0000349 D selected core #0 [soc_target]
0000353 I CPU core #0: Cortex-M7 r1p2, v7.0-M architecture [cortex_m]
0000353 I Extensions: [DSP, FPU, FPU_V5, MPU] [cortex_m]
0000353 I FPU present: FPv5-SP-D16-M [cortex_m]
0000353 D Running task create_components [sequencer]
0000353 D Creating Trace Funnel component [discovery]
0000354 D Creating Trace Funnel component [discovery]
0000355 D Creating Trace Funnel component [discovery]
0000356 D Creating TPIU component [discovery]
0000357 D Creating SWO component [discovery]
0000357 D Creating DWT component [discovery]
0000358 I 4 hardware watchpoints [dwt]
0000360 D Creating FPB component [discovery]
0000360 I 8 hardware breakpoints, 1 literal comparators [fpb]
0000360 D fpb has been disabled [fpb]
0000363 D Creating ITM component [discovery]
0000364 D Running task check_for_cores [sequencer]
0000364 D Running task halt_on_connect [sequencer]
0000364 D halting core 0 [cortex_m]
0000364 D Running task post_connect [sequencer]
0000364 D Running task post_connect_hook [sequencer]
0000364 D Running task create_flash [sequencer]
0000365 D Running task notify [sequencer]
0000365 D set reset catch, core 0 [cortex_m]
0000365 D removing all breakpoints before reset [manager]
0000365 D halting core 0 [cortex_m]
0000366 D reset, core 0, type=VECTRESET [cortex_m]
0000366 D no delegate or debug sequence handled reset; performing VECTRESET reset, core 0 [cortex_m]
0000469 D clear reset catch, core 0 [cortex_m]
0000470 D disabling hardware breakpoints after reset [manager]
0000472 I Loading <path_to_my_hex> [load_cmd]
0000520 D halting core 0 [cortex_m]
0000782 D resuming core 0 [cortex_m]
0000782 D added=[] removed=[] [manager]
0000782 D bps after flush={} [manager]
0000811 D Analyze time: 0.291050 [builder]
0000811 D halting core 0 [cortex_m]
0000815 D resuming core 0 [cortex_m]
0000815 D added=[] removed=[] [manager]
0000815 D bps after flush={} [manager]
0000827 D resuming core 0 [cortex_m]
0000827 D added=[] removed=[] [manager]
0000827 D bps after flush={} [manager]
0000834 D resuming core 0 [cortex_m]
0000835 D added=[] removed=[] [manager]
0000835 D bps after flush={} [manager]
0000842 D resuming core 0 [cortex_m]
0000842 D added=[] removed=[] [manager]
0000842 D bps after flush={} [manager]
0000845 D halting core 0 [cortex_m]
0000854 D resuming core 0 [cortex_m]
0000854 D added=[] removed=[] [manager]
0000854 D bps after flush={} [manager]
0001178 D resuming core 0 [cortex_m]
0001178 D added=[] removed=[] [manager]
0001178 D bps after flush={} [manager]
0001182 D uninit session <pyocd.core.session.Session object at 0x7fb9f7f447d0> [session]
0001182 D uninit board <pyocd.board.board.Board object at 0x7fb9fa9f2660> [board]
0001183 D resuming core 0 [cortex_m]
0001183 D added=[] removed=[] [manager]
0001183 D bps after flush={} [manager]
0001196 C flash program page failure (address 0x00400000; result code 0x1) [__main__]
```
If it is helpful, pyocd can detect both debug probes. here is the output of `pyocd list -v`
```
# Probe/Board Unique ID Target
------------------------------------------------------------------------------------
0 NXP Semiconductors MCU-LINK (r0FB) CMSIS-DAP V3.167 YVIKSUH0XBMF0 n/a
1 Segger J-Link Compact Base 823001019 n/a
```