Need for some explanations regarding PIN configuration tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need for some explanations regarding PIN configuration tool

ソリューションへジャンプ
2,119件の閲覧回数
kyf
Contributor V

Hello NXP team.

I'm developing firmware for S32K341 and S32K344 mcu.

 

I would like to ask:

1. Why are those located in the PIN configuration tool ?

2. Are those configurations regarding RTD drivers ?

3. Why is some pins located in more than one peripheral ?? for example "reset_b" is located both in Platform and in System peripheral.

4. Can you please provide me with training material (other than reference manual) regarding those peripherals ?

 

kyf_0-1662383435308.png

 

 

 

Kind regads,

kyf

0 件の賞賛
返信
1 解決策
2,094件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

 Hi @kyf,

SYSTEM is the peripheral of S32K3, which is described in IOMux.xlsx attached in Reference manual of S32K3XX
PowerAndGround is default peripheral, which is not editable.
Platform is vague in this context, in my opinion, it should be removed from the Pins config tools as it make obscure understanding. I requested development team to process this.
Why is some pins located in more than one peripheral -> It's confirmed as the bug, as 1 pin should choose for 1 peripheral, in this case you should only choose peripheral SYSTEM for this pin

I saw 1 sharing video to use Pins configuration tool as below links, please check it:
Video Getting Started: Pins Tool1598720929958 - NXP Community
Videos for artiom - NXP Community

元の投稿で解決策を見る

4 返答(返信)
2,095件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

 Hi @kyf,

SYSTEM is the peripheral of S32K3, which is described in IOMux.xlsx attached in Reference manual of S32K3XX
PowerAndGround is default peripheral, which is not editable.
Platform is vague in this context, in my opinion, it should be removed from the Pins config tools as it make obscure understanding. I requested development team to process this.
Why is some pins located in more than one peripheral -> It's confirmed as the bug, as 1 pin should choose for 1 peripheral, in this case you should only choose peripheral SYSTEM for this pin

I saw 1 sharing video to use Pins configuration tool as below links, please check it:
Video Getting Started: Pins Tool1598720929958 - NXP Community
Videos for artiom - NXP Community

2,086件の閲覧回数
kyf
Contributor V

Hello @cuongnguyenphu 

 

Thank you for answering my questions. I've tried to open your video link but it seems that I don't have privileges to watch that content.

How can I get access to the video ?

Do I have to gain  access to a service like SafeAssure ?

 

 

Kind regards,

kyf

タグ(1)
0 件の賞賛
返信
2,079件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Let's check this link for alternatively:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Getting-Started-Pins-Tool/ta-p/1130225

I'm not sure if it need any privileges to watch

0 件の賞賛
返信
2,077件の閲覧回数
kyf
Contributor V

This video worked.

Thank you for providing me with this video.

 

 

 

Kind regards,

kyf

0 件の賞賛
返信