NXPS32k148_Ethernet communication with KSZ8061 daughter board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXPS32k148_Ethernet communication with KSZ8061 daughter board

1,826 Views
Milado
Contributor II

Hello ,

I'm using NXPS32k148 and KSZ8061 Ethernet daughter board to enable Ethernet communication with a PC or another device.

I'm using "lwip_s32k148" example but the communication doesn't work for now.

First of all I want to verify if my schematic is ok.

I'll attached the schematic of board.

Can you please confirm that the schematic is ok? or not?

 

Best regards;

Milad

 

0 Kudos
Reply
2 Replies

1,521 Views
peter09
Contributor III

i am using mcp5775b bord with ksz8061 ic i want to print dynamic ip and mac address can any one give me example code 

 

0 Kudos
Reply

1,821 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Milado 

In the following links are the schematics of the S32k148EVB:

S32K148EVB-Q176 Evaluation Board – REV A 

S32K148EVB-Q176 Evaluation Board – REV B 

I believe these would be useful for you.

 

B.R.

VaneB

0 Kudos
Reply