NXP TOUCH SENSE SOLUTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP TOUCH SENSE SOLUTION

Jump to solution
1,829 Views
luosui
Contributor I

请问这两张原理图是属于自容式企业微信截图_16740227762794.png企业微信截图_16740228046443.png方案还是互容式方案

0 Kudos
1 Solution
1,564 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Luo Sui,

Yes, that is correct.

View solution in original post

0 Kudos
6 Replies
1,817 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @luosui,

Which two schematics do you compare here?

 

Thanks,

BR, Daniel

0 Kudos
1,800 Views
luosui
Contributor I

Hi,Daniel:

Here are the SCH files,Can you tell which kind of cap sensing tech they are using? Please inform me the answer,Thank you,BR.

0 Kudos
1,767 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @luosui,

The S32K144 does not have any dedicated touch sense peripheral module, that is why the HW implementation uses GPIO + ADC and two pins per an electrode .

Whereas the KE1xZ MCU has a dedicated TSI module.

 

Regards,

Daniel

0 Kudos
1,593 Views
luosui
Contributor I

Hi,Daniel
According to your description:

1. The S32K144 uses GPIO + ADC and two pins per an electrode ,it is self cap sense tech,right?

2. And the KE1xZ MCU has a dedicated TSI module,so it only need one ADC pin and one electrode to fulfill touch sense function.

 

Regards,

luo sui

0 Kudos
1,565 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Luo Sui,

Yes, that is correct.

0 Kudos
1,560 Views
luosui
Contributor I

Tkanks,BRO,help a lot !

0 Kudos