Multiple PDB trigger output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Multiple PDB trigger output

跳至解决方案
3,781 次查看
Antal
Contributor II

I want to generate multiple triggers for the ADC.
The PDB's input trigger originates from PWM:
Ftm0InitTrig -> Pdb0TrgIn. Relative to this, I want to generate ADC conversion on 600, 1300, 2000, and 2700 clock delays.

I can only make one trigger with (INST_PDB_0, 0, 0, delay) setup.
Did I misunderstand the PDB functions, or am I doing something wrong?

 

void PDB0_init(void)
{
PDB_DRV_Init(INST_PDB_0, &pdb_config_1_timerConfig0);
PDB_DRV_Init(INST_PDB_0, &pdb_config_1_timerConfig1);
PDB_DRV_Init(INST_PDB_0, &pdb_config_1_timerConfig2);
PDB_DRV_Init(INST_PDB_0, &pdb_config_1_timerConfig3);

PDB_DRV_Enable(INST_PDB_0); // enable PDB before LDOK

// config pretriggers on ch0 based on component setting
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig0);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig1);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig2);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig3);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig4);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig5);
PDB_DRV_ConfigAdcPreTrigger(INST_PDB_0, 0UL, &pdb_config_1_adcTrigConfig6);

/* Set PDB0 modulus value */
PDB_DRV_SetTimerModulusValue(INST_PDB_0, 4096);

/* PDB0 pre-trigger0 delays set to sense in the middle of the PWM cycle */

PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 0, 600); // 640 -> 16us, OK
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 1, 1300); // 1300 -> 24us ?
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 2, 2000); // 2400 -> 33.6us ?
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 3, 2700); // 2700 -> 42.4us ?

// PDB_DRV_SetCmpPulseOutDelayForHigh(INST_PDB_0, 0L , 0); // <- PDB0PulseOut signal in TRGMUX
// PDB_DRV_SetCmpPulseOutDelayForLow(INST_PDB_0, 0L, 600); // <- PDB0PulseOut signal in TRGMUX


// PDB_DRV_SetCmpPulseOutEnable(INST_PDB_0, 1<<0, true);

//PDB_DRV_SetValueForTimerInterrupt(INST_PDB_0, 4999); /* Set PDB1 interrupt delay value */

PDB_DRV_LoadValuesCmd(INST_PDB_0); /* Load PDB0 configuration */

}

 

0 项奖励
回复
1 解答
3,705 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the green box represents single ADC channel then you can achieve this by setting individual pretriggers delay. If it represents multiple channels then it can be done by using back-2-back mode, but just 2 multiple conversion can be initiated using both PDB channels.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,754 次查看
Antal
Contributor II

How to do the:
"Do you have pdb_config_1_adcTrigConfign defined with pretrigger index and pretrigger output options enabled?"
Al my configuration is now posted for PDB_0.

0 项奖励
回复
3,756 次查看
Antal
Contributor II

Of these, only the first configuration is active with correct timing for any selected clock delay:

PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 0, 600); // 640 -> 16us, OK

 

Antal_0-1649338824015.png

 


These are not triggering the ADC :
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 1, 1300); // 1300 -> 24us ?
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 2, 2000); // 2400 -> 33.6us ?
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB_0, 0, 3, 2700); // 2700 -> 42.4us ?

I observed the ADC conversion in the ADC0_IRQHandler() using an output pin On/Off during the interrupt execution.

 

 

My setup for this:

---------------------------------------------------------------------------------
/*! @brief ADC pre-trigger configurations */
const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig0 = {
.adcPreTriggerIdx = 0U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = false
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig1 = {
.adcPreTriggerIdx = 1U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig2 = {
.adcPreTriggerIdx = 2U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig3 = {
.adcPreTriggerIdx = 3U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig4 = {
.adcPreTriggerIdx = 4U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig5 = {
.adcPreTriggerIdx = 5U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};

const pdb_adc_pretrigger_config_t pdb_config_1_adcTrigConfig6 = {
.adcPreTriggerIdx = 6U,
.preTriggerEnable = true,
.preTriggerOutputEnable = true,
.preTriggerBackToBackEnable = true
};


/*! @brief PDB timer configurations */
const pdb_timer_config_t pdb_config_1_timerConfig0 = {
.loadValueMode = PDB_LOAD_VAL_IMMEDIATELY,
.seqErrIntEnable = false,
.clkPreDiv = PDB_CLK_PREDIV_BY_1,
.clkPreMultFactor = PDB_CLK_PREMULT_FACT_AS_1,
.triggerInput = PDB_TRIGGER_IN0,
.continuousModeEnable = false,
.dmaEnable = false,
.intEnable = false,
.instanceBackToBackEnable = false,
};

const pdb_timer_config_t pdb_config_1_timerConfig1 = {
.loadValueMode = PDB_LOAD_VAL_IMMEDIATELY,
.seqErrIntEnable = false,
.clkPreDiv = PDB_CLK_PREDIV_BY_1,
.clkPreMultFactor = PDB_CLK_PREMULT_FACT_AS_1,
.triggerInput = PDB_TRIGGER_IN0,
.continuousModeEnable = false,
.dmaEnable = false,
.intEnable = false,
.instanceBackToBackEnable = false,
};

const pdb_timer_config_t pdb_config_1_timerConfig2 = {
.loadValueMode = PDB_LOAD_VAL_IMMEDIATELY,
.seqErrIntEnable = false,
.clkPreDiv = PDB_CLK_PREDIV_BY_1,
.clkPreMultFactor = PDB_CLK_PREMULT_FACT_AS_1,
.triggerInput = PDB_TRIGGER_IN0,
.continuousModeEnable = false,
.dmaEnable = false,
.intEnable = false,
.instanceBackToBackEnable = false,
};

const pdb_timer_config_t pdb_config_1_timerConfig3 = {
.loadValueMode = PDB_LOAD_VAL_IMMEDIATELY,
.seqErrIntEnable = false,
.clkPreDiv = PDB_CLK_PREDIV_BY_1,
.clkPreMultFactor = PDB_CLK_PREMULT_FACT_AS_1,
.triggerInput = PDB_TRIGGER_IN0,
.continuousModeEnable = false,
.dmaEnable = false,
.intEnable = false,
.instanceBackToBackEnable = false,
};

 

0 项奖励
回复
3,744 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you have back-to-back enabled for pretriggers1-7, so its delay is ignored. So disable it thus pretrigger delay can be used
However with back-to-back operation a conversion should be done too.

BR, Petr  

0 项奖励
回复
3,737 次查看
Antal
Contributor II

Hello Petr,
I don't understand your response.
Is the S32K144's PDB hardware support multiple delayed triggers, as the image depicts, or not?
If yes, and you know the solution can you share it with us?
Best Regards,
Antal

ADC_REatTimeControl.png

0 项奖励
回复
3,706 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the green box represents single ADC channel then you can achieve this by setting individual pretriggers delay. If it represents multiple channels then it can be done by using back-2-back mode, but just 2 multiple conversion can be initiated using both PDB channels.

BR, Petr

0 项奖励
回复
3,380 次查看
Jimny
Contributor II

hello @PetrS 

I got the same error.

I want to modify the S32K144 pmsm demo to add more analog signals. The original demo uses adc0 to get 1 analog signal, and adc1 to get 2 analog signals. I want to use adc0 and adc1 to get 3 analog signals respectively, totally 6 analog signals. And the pretrigger delay time is 0, 200, 2000. Please see my thread for detail. Also the project.

https://community.nxp.com/t5/S32-SDK/how-to-config-adc-and-pdb-for-multiple-channels/m-p/1549325

But I got pdb sequency error during debug phase and have no idea on how to solve it. Could you give me some support?

0 项奖励
回复
3,765 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

usage of functions PDB_DRV_ConfigAdcPreTrigger, PDB_DRV_SetAdcPreTriggerDelayValue is correct.
So you do not see ch0DLYn registers written, and triggers does not happen in desired time? 
Do you have pdb_config_1_adcTrigConfign defined with pretrigger index and pretrigger output options enabled?

BR, Petr

0 项奖励
回复