Memset() with RAM segments

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memset() with RAM segments

8,655 Views
ambarishhundeka
Contributor III

Hi NXP team,

I am using S32K144 controller in our project.

I used the meset() with linker script global variables.

 memset(&__FSLCODE_SECTION_START, 0x00, __FSLCODE_SECTION_END - __FSLCODE_SECTION_START);

but that FSL code  segment (section) is not set to zero.

find the attached document for more information on memeset() problem.

Regarding the watchdog timer :

I used the code given in the reference manual for watchdog configuration 

DISABLE_INTERRUPTS(); // disable global interrupt
WDOG->CNT = 0xD928C520; //unlock watchdog
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked
WDOG->TOVAL = 256; //set timeout value
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |
WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect
ENABLE_INTERRUPTS(); //enable global interrupt

if(WDOG->CNT >= 125)
{
DISABLE_INTERRUPTS(); // disable global interrupt
WDOG->CNT = 0xB480A602; // refresh watchdog
ENABLE_INTERRUPTS(); //
}

in the above code , control not come out of the while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0);

Kindly help in this.

Regards,

Ambarish 

Labels (1)
0 Kudos
10 Replies

8,174 Views
wangpengfei
Contributor I

Hi Raju,

//if(timeout_s > 127) return PUBLIC_STATUS_ERROR;
INT_SYS_DisableIRQGlobal();

WDOG->CNT = 0xD928C520; // Unlock WDOG
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0);

WDOG->TOVAL =timeout_ms;//128 * timeout_s; // Timeout in max = 65535 * (1 / 1 kHz) = 65535ms
//WDOG->CS = WDOG_CS_EN(1)|WDOG_CS_CLK(1)|WDOG_CS_INT(1)|WDOG_CS_WIN(0)|WDOG_CS_UPDATE(0);
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) | WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0) | WDOG_CS_DBG(1);

while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0);
INT_SYS_EnableIRQGlobal();

 It's stuck here

while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0);

0 Kudos

8,174 Views
bjrajendra
Senior Contributor I

Hi Wang,

If you are trying to update/ reconfigure the watchdog after initial watchdog configuration like initial disable watchdog function or something 

I suggest you use WDOG_CS_UPDATE(1) in your initial watchdog configuration.

Raju

0 Kudos

8,174 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Regarding the watchdog, the code works on my side with both masksets (0N47T, 0N57U) as expected.

There is a restriction that the reconfiguration must be done within 128 bus cycles.

So you cannot step the code. 

Regards,

Daniel 

0 Kudos

8,174 Views
ambarishhundeka
Contributor III

@Hello Daniel,

Thank you for your support.

could you please share your complete tested source code.

I tried with toggling the LED while  refreshing the  watchdog , but LED is not toggling.

directly flashed the code and checked.

EVAL board has PS32K144HFVLL 0N77P controller chip.

 

PCC-> PCCn[PCC_PORTD_INDEX] = PCC_PCCn_CGC_MASK; /* Enable clock for PORT D */

PTD->PDDR |= 1<<0; /* Port D0: Data Direction= output */

PORTD->PCR[0] = 0x00000100; /* Port D0: MUX = ALT1, GPIO (to blue LED on EVB) */ WDOG->CNT = 0xD928C520; //unlock watchdog

DISABLE_INTERRUPTS();

while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked

WDOG->TOVAL = 0x1E8480; // used the default clock  configuration , not configured clock in the code //set the count to 2000000

WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |

WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);

while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect

ENABLE_INTERRUPTS(); //enable global interrupt

while(1)

{

//PTD->PDDR = 1;

if(WDOG->CNT >= 0xF4240) //if count  is equal or greater 1000000

{

DISABLE_INTERRUPTS(); // disable global interrupt

WDOG->CNT = 0xB480A602; // refresh watchdog

ENABLE_INTERRUPTS(); //

PTD->PTOR |= 1<<0;

}

}

Thanks,

Ambarish

0 Kudos

8,174 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Ambarish,

The problem is in the maskset (0N77P).
Please use either 0N47T or preferably 0N57U which is the production version.
There are many differences between 0N77P and 0N47T/0N57U.

The current RM is not compatible with that maskset.

WDOG_CS[ULK] is not present on 0N77P thus it reads 0.

pastedImage_1.png

Regards,

Daniel

0 Kudos

8,174 Views
bjrajendra
Senior Contributor I

Hi Daniel,

Is there any similar issue with S32K142.

Raju

0 Kudos

8,174 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

No, there is no such issue with the S32K142.

There is only one S32K142 mask 0N33V covered by the S32K1xx RM, DS.

BR, Daniel

0 Kudos

8,174 Views
bjrajendra
Senior Contributor I

Hi Daniel,

Thanks for the response.

I'm trying to implement the watchdog code and the code just has a while(1) loop with the below code. I expect the code will reset so I set a breakpoint at the start of the code to ensure the reset. But it still there is no reset happened. 

DISABLE_INTERRUPTS();

WDOG->CNT = 0xD928C520; //unlock watchdog

while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked

WDOG->TOVAL = 256; // used the default clock configuration , not configured clock in the code //set the count to 2000000

WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |

WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);

while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect

ENABLE_INTERRUPTS(); //enable global interrupt

Kindly suggest us a solution 

Raju.

0 Kudos

8,174 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

So the core stays halted at the breakpoint?

You can enable the WDOG in the debug mode of the MCU.

WDOG_CS[DBG] = 1

BR, Daniel

8,174 Views
bjrajendra
Senior Contributor I

Thanks Daniel. It is working now. Thanks for the support.

Raju

0 Kudos