Making use of S32K344 RTD MCAL/driver calls to Det_ReportError

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Making use of S32K344 RTD MCAL/driver calls to Det_ReportError

902件の閲覧回数
JayAtlis
Contributor II

Hello,

I’m adding some general error handling into the firmware for my company’s S32K344-based ECM. I see various NXP MCAL/drivers code calling into the AUTOSAR Det_ReportError interface with meaningful information. I’d like to capture that information for logging.  According to the AUTOSAR DET documentation there’s supposed to be a way to register callbacks that I’d think would be appropriate to accomplish the desired logging, however it doesn’t seem that NXP’s version of DET is supporting this? The implementation in RTD/src/Det.c appears to be only a stub that simply sets some variables in memory and returns without doing anything more.

Is there something I’m missing? Is there some way I should be able to get the usage of Det_ReportError from NXP's MCAL/drivers to actually do something useful (e.g. callout to logging function)?

Thanks.

タグ(5)
0 件の賞賛
3 返答(返信)

888件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Unfortunately, we don't have any implementation for DET. It is a responsibility of integrators to decide what to do next with the reported error. I would suggest that in Det_ReportError function, you can simply log the error code to a console. 

Best Regards,

Nam

0 件の賞賛

879件の閲覧回数
JayAtlis
Contributor II

The challenge is, RTD/src/Det.c is generated code, and I'm not sure the peripheral configuration tool lets us turn this one off. So even if I edit the function as you suggest, it would get overwritten the next time peripheral configuration changes and code gets generated again. It isn't a __weak__ function either so I can't just replace it with my own function of the same name.

I ended up using GCC linker's --wrap option so, any calls to Det_ReportError go to my own implementation named __wrap_Det_ReportError.

0 件の賞賛

865件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @JayAtlis,

I see. The point is the driver code is refreshed every code generation, and the code modified in e.g. RTD/src/Det.c will be overwritten by the original code imported from the Platform SDK. You can get rid of it by directly modifying the code from Platform SDK, e.g. C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203\Det_TS_T40D34M20I0R0\src\Det.c

namnguyenviet_0-1660880443161.png

After that, re-generate the code to take effect.

namnguyenviet_1-1660880499249.png

 

Best Regards,

Nam

0 件の賞賛