MCSXTE2BK142 single shunt code can't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCSXTE2BK142 single shunt code can't work

ソリューションへジャンプ
2,291件の閲覧回数
peter_shi
Contributor II
MCSXTE2BK142\sw\MCSXTE2BK142_PMSM_FOC_1Sh
0 件の賞賛
返信
1 解決策
2,197件の閲覧回数
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,261件の閲覧回数
peter_shi
Contributor II

Hi,

I bought 1 pcs MCSXTE2BK142 demo board from your Website and download the demo code from the website as well.

When I used the two-shunt resistance, the function is ok. I could run motors. 

For the single-shunt demo code, I removed C68, C70, and C65 to check the function.  VF function is ok. But when I used sensor-less control, the motor can't run even if it was in open loop stage.

I checked the demo code about ADC configuration, I found the ADC configuration was wrong. The demo code used CH8, but Hardware used CH15.

I reconfigured the ADC channel, but it still doesn't work. FreeMaster report phase over current. I think dc-current sampling has some issue.

 

0 件の賞賛
返信
2,021件の閲覧回数
Shrikant1
Contributor I

i am not able to run it in dual shunt specifically in closed loop. Have you tried with sensoed or sensor less which type of sensor you have used.

0 件の賞賛
返信
2,198件の閲覧回数
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

0 件の賞賛
返信
2,207件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

I'm sorry for the delay.

It looks like you are right, but the issue is still under investigation.

 

BR, Daniel

0 件の賞賛
返信
2,269件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

Can you be more specific?

What error does the FreeMaster report?

 

BR, Daniel

0 件の賞賛
返信