MCSXTE2BK142 single shunt code can't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSXTE2BK142 single shunt code can't work

Jump to solution
2,166 Views
peter_shi
Contributor II
MCSXTE2BK142\sw\MCSXTE2BK142_PMSM_FOC_1Sh
0 Kudos
Reply
1 Solution
2,072 Views
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

View solution in original post

0 Kudos
Reply
5 Replies
2,136 Views
peter_shi
Contributor II

Hi,

I bought 1 pcs MCSXTE2BK142 demo board from your Website and download the demo code from the website as well.

When I used the two-shunt resistance, the function is ok. I could run motors. 

For the single-shunt demo code, I removed C68, C70, and C65 to check the function.  VF function is ok. But when I used sensor-less control, the motor can't run even if it was in open loop stage.

I checked the demo code about ADC configuration, I found the ADC configuration was wrong. The demo code used CH8, but Hardware used CH15.

I reconfigured the ADC channel, but it still doesn't work. FreeMaster report phase over current. I think dc-current sampling has some issue.

 

0 Kudos
Reply
1,896 Views
Shrikant1
Contributor I

i am not able to run it in dual shunt specifically in closed loop. Have you tried with sensoed or sensor less which type of sensor you have used.

0 Kudos
Reply
2,073 Views
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

0 Kudos
Reply
2,082 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

I'm sorry for the delay.

It looks like you are right, but the issue is still under investigation.

 

BR, Daniel

0 Kudos
Reply
2,144 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

Can you be more specific?

What error does the FreeMaster report?

 

BR, Daniel

0 Kudos
Reply