MC33771C BMS Driver for S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C BMS Driver for S32K344

Jump to solution
1,798 Views
JoDo
Contributor III

Hi, we are currently working on a BMS application with the MC33771C analog front end that will communicate with the S32K344 controller via TPL. I have researched but could not find any drivers or smaple projects suitable for the S32K3 controller, only for the S32K1.

Are these available anywhere or in the planning stages?

There was also a BMS software reference design announced for the S32K3 controller, is there a date when it will be released?

JoDo_0-1640853884974.png

Regards,

JoDo

 

0 Kudos
Reply
1 Solution
1,763 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Johannes,

The BMS reference design with the new S32K3 MCU and latest MC33775 BCC is planned to be released in Q2 2022. As part of this ref design will be a driver for the MC33775 only.

If you intend to use the MC33771C, you will have to port the driver available for the S32K1. It should be pretty easy by changing low-level layer for SPI and DMA.

Best regards,

Tomas

View solution in original post

2 Replies
1,573 Views
NewStarter
Contributor II

Hi NXP supportors,

 I bought 2 EVBs  of https://www.nxp.com/design/designs/rd33771-48vevm-reference-design:RD33771-48VEVM#Design-Resources and facing an issue that from its schematics I can't find where is the current path when I connect a battery pack or using a slider battery pack emulator.

search VB_ISENSE_+ or VB_ISENSE_- but got nothing from

RD33771-48VEVM Schematics

NewStarter_0-1648632456286.png

 

0 Kudos
Reply
1,764 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Johannes,

The BMS reference design with the new S32K3 MCU and latest MC33775 BCC is planned to be released in Q2 2022. As part of this ref design will be a driver for the MC33775 only.

If you intend to use the MC33771C, you will have to port the driver available for the S32K1. It should be pretty easy by changing low-level layer for SPI and DMA.

Best regards,

Tomas