MAC address of S32K controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAC address of S32K controller

774件の閲覧回数
rak14
Contributor III

Hi,

I'm using multiple S32K148 controllers with Ethernet feature.

In example code lwip_S32K148 the MAC address is .hwaddr = { 0x10, 0x11, 0x12, 0x77, 0x77, 0x77 }.
Can we change the MAC address to different for different controllers?

Is there any constrain to use the particular Mac address?

0 件の賞賛
返信
1 返信

754件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes you can, or better you should. Each device on your LAN should have unique MAC address.

Check web for MAC address composition.

BR, Petr

0 件の賞賛
返信