Low power and Doze Mode question in S32K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low power and Doze Mode question in S32K

2,180 Views
aiguo_sun
Contributor I

In S32K RM,I found these LPSPI/LPUART/LPI2C peripherals. I know LP stand for Low Power,but I did not understand what is the difference between LPSPI and normal SPI?

Also there is 'DOZEN' in the register of LPSPI(also LPI2C/LPSPI/FlexIO),

pastedImage_1.png

What does Doze mode mean?

B.R.

Terry Sun

2 Replies

1,998 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Terry Sun,

Regarding your questions please see my comments below: 

What is the difference between LPSPI and normal SPI?

There are two important points of the Low Powe peripherals comparing to the standard peripherals: 

  • The LP modules are designed to use little CPU overhead.
  • The LP modules can continue operating in stop modes if an appropriate clock is available.

What does Doze mode mean?

Doze mode is like stop mode for the modules. For example, for the LPSPI, the DOZEN bit by default is zero, this means that if you send the MCU to a stop mode, the module will continue working as long as it has an appropriate clock. If you set the DOZEN bit and you send the module to a stop mode, the module won't work. 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,998 Views
aiguo_sun
Contributor I

Thanks very much!

B.R.

Terry Sun

0 Kudos
Reply