Lock up event on Flash partitioning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Lock up event on Flash partitioning

2,139 次查看
sabeelmohamedkh
Contributor I

Hi

In reference on S32K148 controller, we are trying to partition the flash area into 1.5MB of code flash and remaining 512Kk region as a FlexNvm, After execution the programming sequence to program FlexNvm , we are obtaining Resets due to LOCKUP event.

Could you please share on the reasons for the same.

0 项奖励
回复
3 回复数

1,965 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Do you launch the program partition command from RAM?

Regards,

Daniel

0 项奖励
回复

1,965 次查看
andreaolivieri
Contributor I

Hi Daniel.

Your response triggered my another question.

Is the partitioning command a procedure which has to be execute through executable code located in RAM?

Shall I have to perform an overlay?

I'm asking so because in the device's RM (Rev. 6, 12/2017) I noticed this recommendation in § "35.5.11.14 Program Partition command" which states :

"...

Program Partition command must not be launched from flash memory, since flash memory resources are not accessible during Program Partition command execution.

..."

0 项奖励
回复

1,965 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Andrea,

Answered here::Program Partition 

BR, Daniel

0 项奖励
回复