Link error while building S32K14X MCAL Sample Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Link error while building S32K14X MCAL Sample Application

2,539 次查看
anbunathanr
Contributor I

I am trying to build S32K14X MCAL Sample Application as per the attached PDF file

 

I have compiled the code by adding

#define MCAL_ENABLE_USER_MODE_SUPPORT 1
in
cfg/include/CDD_Mcl_Cfg.h
cfg/include/Can_Cfg.h
cfg/include/Fls_Cfg.h
cfg/include/Gpt_Cfg.h
cfg/include/Mcu_Cfg.h

 

I am trying to build using the command inside build.bat: (refer attached 7z file)

call launch.bat TOOLCHAIN=linaro MODE=SUPR DERIV=144

 

But I am getting following link errors:

Kindly help to resolve these issues.

 

c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: warning: bin/sample_app_mcal.elf has a LOAD segment with RWX permissions
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Can.o: in function `Can_Init':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:471: undefined reference to `Sys_GoToSupervisor'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:471: undefined reference to `Sys_GoToUser_Return'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Can.o: in function `Can_ChangeBaudrate':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:590: undefined reference to `Sys_GoToSupervisor'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:590: undefined reference to `Sys_GoToUser_Return'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Can.o: in function `Can_SetControllerMode':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:757: undefined reference to `Sys_GoToSupervisor'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:757: undefined reference to `Sys_GoToUser_Return'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Can.o: in function `Can_MainFunction_BusOff':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:2005: undefined reference to `Sys_GoToSupervisor'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:2005: undefined reference to `Sys_GoToUser_Return'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Can.o: in function `Can_MainFunction_Mode':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:2105: undefined reference to `Sys_GoToSupervisor'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Can_TS_T40D2M10I0R0/src/Can.c:2105: undefined reference to `Sys_GoToUser'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Fls_Flash.o: in function `Fls_Flash_VerifyWrite':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Fls_TS_T40D2M10I0R0/src/Fls_Flash.c:1237: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Fls_Flash.o: in function `Fls_Flash_VerifyErase':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Fls_TS_T40D2M10I0R0/src/Fls_Flash.c:1044: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Fls_Flash.o: in function `Fls_Flash_SectorRead':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Fls_TS_T40D2M10I0R0/src/Fls_Flash.c:3033: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Fls_Flash.o: in function `Fls_Flash_SectorCompare':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Fls_TS_T40D2M10I0R0/src/Fls_Flash.c:3407: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_Init':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:405: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:409: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:413: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_InitClock':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:439: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:447: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:455: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:462: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:468: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:475: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:482: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_SetMode':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:581: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:585: undefined reference to `Mcal_Trusted_Call'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_GetResetReason':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:663: undefined reference to `Mcal_Trusted_Call_Return'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_Init':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:416: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_InitClock':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:487: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_DistributePllClock':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:514: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_SetMode':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:618: undefined reference to `Mcal_Trusted_Call1param'
c:/toolchain/gcc-arm-none-eabi/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: ./bin/Mcu_IPW.o: in function `Mcu_Ipw_GetResetRawValue':
C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins/Mcu_TS_T40D2M10I0R0/src/Mcu_IPW.c:683: undefined reference to `Mcal_Trusted_Call_Return'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:230: bin/sample_app_mcal.elf] Error 1

 

 

 

0 项奖励
回复
2 回复数

2,478 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please do not manually modify the generation code. Instead, please configure user mode in EB Tresos GUI. Besides, build the app with MODE=SUPR means MCAL_ENABLE_SUPERVISOR_MODE is defined, not MCAL_ENABLE_USER_MODE_SUPPORT.

Best Regards,

Nam

0 项奖励
回复

2,476 次查看
anbunathanr
Contributor I

Thanks.

We solved this issue by selecting right combination as follows:

SET TRESOS_DIR=C:/EB/tresos23
SET MAKE_DIR=C:/NXP/S32DS_ARM_v2018.R1/utils/msys32/usr
SET GCC_DIR=C:/GNUArmEmbeddedToolchain/102021.10
SET LINARO_DIR=C:/GNUToolsARMEmbedded/62017-q2-update

SET PLUGINS_DIR=C:/NXP/AUTOSAR/S32K14X_MCAL4_2_RTM_1_0_0/eclipse/plugins

0 项奖励
回复