Ld error: Cannot run program "": Launching failed C/C++ Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ld error: Cannot run program "": Launching failed C/C++ Problem

6,257 次查看
475824827
Contributor I

Why do I always get this error when build the project?

捕获.JPG

but I can get the right .elf and .bin files.

Does this have any effect?

标记 (2)
0 项奖励
回复
8 回复数

5,837 次查看
475824827
Contributor I

Thank you. I've solved that problem. I just reinstall the S32DS software.

0 项奖励
回复

5,838 次查看
hejc1996
Contributor I

Hello,

I have this problem ,too. Do you know why? And where is the second installation?thanks.

0 项奖励
回复

5,838 次查看
jiri_kral
NXP Employee
NXP Employee

Hi,

what is your S32DS version? Are you using built-in example or you are trying import older project?

Jiri

0 项奖励
回复

5,769 次查看
bjrajendra
Senior Contributor I

Hi jiri,

 

We are facing the similar scenario and getting this ld error. Could you help in resolving this issue.

 

Thanks,

Raju

0 项奖励
回复

5,838 次查看
475824827
Contributor I

hello

Version:

S32 Design Studio for ARM

Version: 2018.R1
Build id: 180326

(c) Copyright Freescale Semiconductor 2016. All rights reserved.
(c) Copyright NXP 2017-2018.

Visit http://www.nxp.com/

This is the project that I build.

0 项奖励
回复

5,838 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

What's the project you are trying to build? Can you share output from build console? 

Jiri 

0 项奖励
回复

5,004 次查看
alan_yu
Contributor II

hello jiri, 

I meet the same problem too, I can build the example project successfully. but when i import my old project ,i meet the same problem like below picture show . 

alan_yu_2-1647568148386.png

 

alan_yu_1-1647568136730.png

 

thanks ,alan.

 

0 项奖励
回复

4,587 次查看
yuan_luo
Contributor I

hello alan:

 do you solve this problem? i meet the same problem too.

thanks!

0 项奖励
回复