LPUART FIFO size? Only seems to be 4 words.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUART FIFO size? Only seems to be 4 words.

Jump to solution
2,731 Views
fredericksoo
Contributor II

hello,

I'm setting the LPUART FIFO RX and TX sizes and it only seems to be 4 words (0b001) and cannot be set to any other value.  In the RM it says that it can be up to 256 words (up to 0b111).  I've verified that I can set the RXFE, RXTE and RXIDEN bits properly. 

// disable transmit and receive so can set FIFO

LPUART1->CTRL &= !( LPUART_CTRL_TE_MASK | LPUART_CTRL_TE_MASK);

// set fifo - 1 word RX, 32 dataword TX, TX and RX FIFO enabled, 1 byte idle before RDRF transmit

LPUART1->FIFO = LPUART_FIFO_RXFIFOSIZE(0b000) | LPUART_FIFO_TXFIFOSIZE(0b100) | LPUART_FIFO_TXFE(0x01) | LPUART_FIFO_RXFE(0x01) | LPUART_FIFO_RXIDEN(0x01);

When I check with debugger, only RXFE, RXTE and RXIDEN bits are set, the RXFIFOSIZE and TXFIFOSIZE are both 0b001 (both starting values and after trying to set).

Does the LPUART support FIFO depths of anything besides 4 words?

best,

Fred

0 Kudos
Reply
1 Solution
2,497 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The S32Kxx devices support only 4-word FIFO.

See Table 48-1. LPUART instances and features

 

Regards,

Daniel

View solution in original post

2 Replies
2,497 Views
fredericksoo
Contributor II

great, thank you - understand now that it is a read-only field which indicates the FIFO size (not a way to set FIFO size).

0 Kudos
Reply
2,498 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The S32Kxx devices support only 4-word FIFO.

See Table 48-1. LPUART instances and features

 

Regards,

Daniel