Issue with LPUART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with LPUART

1,536 Views
pankajprasad100
Contributor III

Hi,

   I am working with S32K116 in which using example code for LPUART.

While checking the signals using oscilloscope i can see highs and lows but the voltage levels are in 250 to 300 mV range.

Well i think voltage levels should be should be in volts not in milli volts.

Any reason behind it?

 

Thanks & Regards

PANKAJ PRASAD

Tags (1)
0 Kudos
Reply
3 Replies

1,529 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Pankaj,

Which LPUART examples do you use?

Do you have an EVB or your custom board?

Which pins do you scope?

The voltage levels depends on the power supply as you can see in the DS, rev.13, Chapter 5, I/O parameters.

 

Regards,

Daniel

0 Kudos
Reply

1,515 Views
pankajprasad100
Contributor III

1.lpuart echo s32k116

2.custom board

3.rx-PTC2   tx-PTC3

 

0 Kudos
Reply

1,486 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Pankaj,

The issue was reportedly solved.

If not, let me know.

 

Regards,

Daniel

 

0 Kudos
Reply