hi community
At first, the project edited on the S32DS Platform 3.4 with S32K1XX RTM 4.0.3 , and now running on the S32DS Platform 3.4 with S32K1XX RTM 4.0.2 , it cannot be compiled .
My work environment is not connected to the Internet, so I can't load it on the S32DS Platform 3.4_ Extensions and Updates .
Is there any sdk package that contains S32K1XX RTM 4.0.3 ? Just like "SW32K1_S32DS_3.4.1_D2106" contains S32K1XX RTM 4.0.2 . Then, i load sdk with 4.0.3 through S32DS Platform 3.4_Install new software .
Thank for your help !
Hi,
I think updatesite package is not given for it, just standalone version with exe.
You should go through Extensions and Updates, S32 SDK for S32K1xx RTM 4.0.3 would be visible in S32DS 3.4.
BR, Petr