Hi,
I am looking to program using JTAG on a board based on the S32K148EVB. Is there a list of supported JTAG programmers that will work on the dev board that I can test before I make my new board design? To prove the programmer works and therefore will on my new one?
Thanks!
Hi Poley,
Do you mean that you want a list of external debugger programmer?
P&E Universal Multilink and Universal Multilink FX are recommended.
But S32K148 Debug Connector(J10) is standard 20-pin Cortex Debug D ETM connector, so I think almost all debuggers that support Cortex M series should be able to support S32K148.(for example: SEGGER J-Link\ I-JET \ ULINK...)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @Robin_Shen
What Cortex M (3 or 4 for example) needs to be supported for it to work with S32K148?
Will this work with S32DS to program my board?:
https://uk.farnell.com/mikroelektronika/mikroe-1100/debugger-mikroprog-stm32/dp/2281670
Thanks!
I am not able to open this link. Would you please let me know what it? The keyword in that link seems for STM32.
It's this:
Please contact mikroe about whether S32K148 is in the support list. After input S32K148, it seems not in the support list.