Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

ソリューションへジャンプ
1,213件の閲覧回数
snaku_lee
Contributor IV

Hi,

I am using S32K3xx MCU, and the HSE FW(v2.1.0) is installed (enabled), my question is it posibble to advance the life cycle to OEM_PROD without program ADKP ? 

why I asking becuase I changed the life cycle to OEM, but I did not call Csm_SetHSEAttribute() to set the HSE_APP_DEBUG_KEY.

タグ(3)
0 件の賞賛
返信
1 解決策
1,163件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @snaku_lee 

Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided.

 

BR, VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,164件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @snaku_lee 

Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided.

 

BR, VaneB

0 件の賞賛
返信
1,181件の閲覧回数
snaku_lee
Contributor IV
I forgot to say that, the original life cycle is "Simulated_OEM_PROD", not "CUST_DEL". Is that possible to change the LC to OEM without ADKP in the "Simulated_OEM_PROD" life cycle?
0 件の賞賛
返信