Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

跳至解决方案
1,174 次查看
snaku_lee
Contributor IV

Hi,

I am using S32K3xx MCU, and the HSE FW(v2.1.0) is installed (enabled), my question is it posibble to advance the life cycle to OEM_PROD without program ADKP ? 

why I asking becuase I changed the life cycle to OEM, but I did not call Csm_SetHSEAttribute() to set the HSE_APP_DEBUG_KEY.

标记 (3)
0 项奖励
回复
1 解答
1,124 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @snaku_lee 

Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided.

 

BR, VaneB

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,125 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @snaku_lee 

Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided.

 

BR, VaneB

0 项奖励
回复
1,142 次查看
snaku_lee
Contributor IV
I forgot to say that, the original life cycle is "Simulated_OEM_PROD", not "CUST_DEL". Is that possible to change the LC to OEM without ADKP in the "Simulated_OEM_PROD" life cycle?
0 项奖励
回复