解決済! 解決策の投稿を見る。
Hello,
1. I am currently using the TCM of S32K312,
The reason is that only core has direct access as master. Other masters like DMA need to access the TCM memory via backdoor.
2. If I use ITCM_0 Backdoor and DTCM_0 Backdoor, do I need to add definitions in the MEMORY and SECTION sections of linker_flash_s32k312.ld?
Does anyone know where I can obtain a demo for accessing ITCM and DTCM using the Backdoor method?
You can have a look at the example here.
https://community.nxp.com/t5/S32K/DTCM-ITCM-example/m-p/1606827#M21008
Best regards,
Peter
Hello,
1. I am currently using the TCM of S32K312,
The reason is that only core has direct access as master. Other masters like DMA need to access the TCM memory via backdoor.
2. If I use ITCM_0 Backdoor and DTCM_0 Backdoor, do I need to add definitions in the MEMORY and SECTION sections of linker_flash_s32k312.ld?
Does anyone know where I can obtain a demo for accessing ITCM and DTCM using the Backdoor method?
You can have a look at the example here.
https://community.nxp.com/t5/S32K/DTCM-ITCM-example/m-p/1606827#M21008
Best regards,
Peter
Hi @petervlna
Thank you for your response to my post.
Best regards,
Chris