Hi team
As stated in the subject , Initially I explored SPI communication with sample example code "S32K144_Project_LPSPI" , where SPI communication is established between microcontroller & UJA1169TK\F
So now to get familiar with SPI SDK , I tried implementing the same with the help of SDK( PFA processor expert)
Once after generating processor expert code , I used LPSPI_DRV_MasterTransferBlocking API to send & receive data through SPI
uint8_t masterDataSend[2]={0xFD,0x00};
uint8_t masterDataReceive[2];
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
LPSPI_DRV_MasterInit(LPSPICOM1,&lpspiCom1State,&lpspiCom1_MasterConfig0);
LPSPI_DRV_MasterTransferBlocking(LPSPICOM1,&masterDataSend[0],&masterDataReceive[0],2U,10U);
So basically I was expecting value 0xFD & 0x EF in masterDataReceive[0] and masterDataReceive[1] respectively , but I'm receiving zero in masterDataReceive[0] & [1]
To check whether the selected configuration is correct , I used normal non-sdk code to verify processor expert configuration ( Shown below)
uint16_t LPSPI1_16bits_read;
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
LPSPI_DRV_MasterInit(LPSPICOM1,&lpspiCom1State,&lpspiCom1_MasterConfig0);
while((LPSPI1->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0);
/* Wait for Tx FIFO available */
LPSPI1->TDR = 0xFD00; /* Transmit data */
LPSPI1->SR |= LPSPI_SR_TDF_MASK; /* Clear TDF flag*/
while((LPSPI1->SR & LPSPI_SR_RDF_MASK)>>LPSPI_SR_RDF_SHIFT==0);
/* Wait at least one RxFIFO entry */
LPSPI1_16bits_read= LPSPI1->RDR; /* Read received data */
LPSPI1->SR |= LPSPI_SR_RDF_MASK; /* Clear RDF flag*/
With the above code , I could see 0xFDEF in LPSPI1_16bits_read variable , from that I could conclude that there is no issue with processor expert configuration
I'm suspecting I might have sent wrong paramters for LPSPI_DRV_MasterTransferBlocking API , Please let me know if something is wrong
解決済! 解決策の投稿を見る。
Hello @KARTHKSARODE,
Thank you for the project.
It depends on how the data are placed in the memory.
I get good results if I do this:
uint16_t masterDataSend[1]={0xFD00};
uint16_t masterDataReceive[1];
status=LPSPI_DRV_MasterTransferBlocking(LPSPICOM1,(uint8_t*)&masterDataSend[0],(uint8_t*)&masterDataReceive[0],2U,10U);
Regards,
Daniel
Hi @KARTHKSARODE,
Can you please read the error code that the function returns?
Have you scopped the bus?
BR, Daniel
Thanks for the response
Function returns STATUS_SUCCESS
Sadly I don't have any scope with me to test the bus , from the code snippet can you find any error??
Hi @KARTHKSARODE,
I don't see any issues in the code you posted.
Can you share the project so that I can reproduce it on my side?
Regards,
Daniel
After modifying from uint8_t masterDataSend[2]={0xFD,0x00} to uint8_t masterDataSend[2]={0x00,0xFD}
I'm able to receive data masterDataReceive[0]=0xEF & masterDataReceive[1]=0xFD
Why is it working for this combination , can you provide feedback on this ??
Hi @KARTHKSARODE,
If you have a test project, please share it.
I'm not able to reproduce it.
Regards,
Daniel
Hello @KARTHKSARODE,
Thank you for the project.
It depends on how the data are placed in the memory.
I get good results if I do this:
uint16_t masterDataSend[1]={0xFD00};
uint16_t masterDataReceive[1];
status=LPSPI_DRV_MasterTransferBlocking(LPSPICOM1,(uint8_t*)&masterDataSend[0],(uint8_t*)&masterDataReceive[0],2U,10U);
Regards,
Daniel