If I don't use FIRC, should FIRCREGOFF be set to 1? Will it reduce power consumption?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

If I don't use FIRC, should FIRCREGOFF be set to 1? Will it reduce power consumption?

450 次查看
PYGC
Contributor II

PYGC_0-1677132161087.png

 

0 项奖励
回复
1 回复

441 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

The FIRCREGOFF bit is used to control an internal regulator used by the FIRC internal circuit. In order to guarantee the operation frequency of the FIRC at voltage levels higher than 3V, the application must be sure to set this bit. Otherwise, FIRC operational frequency may get out of spec.

If you don't use FIRC, I think you can set FIRCREGOFF=1 for power saving purposes.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复