I2C with s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C with s32k144

215 Views
gopi13
Contributor I

S32K144EVB-Q100 Board I2c master send data but slave not receiving data why ? check my code and give solution (slave is RTC address is 0x68).

0 Kudos
3 Replies

203 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It is recommended to install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
Or install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.
It contains sample projects of I2C master or Slave. Please test these projects and modify the address or baud rate based on your sensor.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Tags (1)
0 Kudos

164 Views
gopi13
Contributor I

hi @Robin_Shen i will try but not working could you help me please . you have any codes send me 

0 Kudos

153 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you use a logic analyzer to observe that the I2C waveform sent by S32K144? Does it meets the requirements of the RTC manual? 
Did S32K144 successfully configure slave device RTC through I2C?
Did S32K144 successfully read the RTC time?
What is the part number of slave device RTC?

0 Kudos