Hi All,
I want to test I2C functionality in S32K148 EVB Rev B board. Could you please help in pointing out which peripheral(s) on the board can be used for testing the same?
Also are there any links for application code which are written specifically for this EVB?
Regards,
Guru
Solved! Go to Solution.
Hi Guru,
Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.
You may need to test the I2C functionality by using two boards or logic analyzer.
You can download Schematics and User Manual of S32K148EVB from here.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks, Robin
Hi Guru,
Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.
You may need to test the I2C functionality by using two boards or logic analyzer.
You can download Schematics and User Manual of S32K148EVB from here.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------