Hello,
I am implementing an i2c demo example to receive data from a sensor,
the s32k144 will act as a master and the sensor as a slave,
I tried to use an example code but all I found was Master Transmitter codes,
is there a simple Master Receiver code available?
Thank you,
Dema.
Solved! Go to Solution.
Hi Dema,
It looks like you are referring to the S32K144_Project_LPI2C example in AN5413SW.
Please install S32DS v3.4 + S32K1 SDK RTM v4.0.3, there are several I2C examples for reference.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Dema,
It looks like you are referring to the S32K144_Project_LPI2C example in AN5413SW.
Please install S32DS v3.4 + S32K1 SDK RTM v4.0.3, there are several I2C examples for reference.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you, Robin,
the sensor was detected and I received an ACK.