I2C Communication on S32K312EVB-Q172 with SDK 3.0 and 5.0 not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Communication on S32K312EVB-Q172 with SDK 3.0 and 5.0 not working

130 Views
Ajit11
Contributor I

Hello There,

I wanted establish I2C communication between S32K312EVB-Q172 and one Peripheral device. I could able to communicate with the peripheral device Using SDK V2.0.3 in both Async and Sync Approaches. I have configured I2C0 pins, Port with proper MSCR number, Platform to enable interrupt and enabled clock from MCU peripheral clock section.

The same configuration created using SDK 3.0 and 5.0 But I could not able to communicate with the peripheral device. can you please Support on this ? are there any I2C specific modification between SDK 2.0.3, 3.0 and SDK 5.0 that not letting to establish communication ? 

Thanks 

Ajit  

 

0 Kudos
Reply
1 Reply

121 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ajit,

Please send me the RTD5.0.0 based project for check.

Refer to: Example S32K312 I2C Transmit & Receive Using DMA DS3.5 RTD300

Best Regards,
Robin

0 Kudos
Reply