I was looking S32K SDK ADC example for hardware and software trigger.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I was looking S32K SDK ADC example for hardware and software trigger.

2,981 Views
hannan_shaikh
Contributor I

The readme file says: You need to connect PTC7 to J20-2 and PTC6 to J20-5 in order to use the onboard RS232 to USB converter. I don't see J20 on the S32K evaluation board. Am I missing anything?

Labels (1)
0 Kudos
Reply
2 Replies

2,481 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I can see that this description is written for validation board (not EVB) which has J20 pin header. S32K144 EVB does not have this jumper.

Regards,

Lukas

0 Kudos
Reply

2,481 Views
hannan_shaikh
Contributor I

Hi Lukas,

Thank you very much for your response. Is there any other option I could use to test same ADC example on S32K144EVB.

Regards,

Hannan

0 Kudos
Reply