I can't find LPSPI_DRV_SetPcs() in the component window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't find LPSPI_DRV_SetPcs() in the component window

Jump to solution
1,749 Views
Zyuan17
Contributor III

Zyuan17_0-1666318541267.png

Zyuan17_1-1666318619497.png

 

I am using S32K142EVB to build a project. But there is an API in the example code is not included in the components window.

 

Tags (1)
0 Kudos
Reply
1 Solution
1,735 Views
Zyuan17
Contributor III

Zyuan17_0-1666343268137.png

Hi Robin, I still can't find this API in the document and in the component window after I open the Oxygen document.

 

View solution in original post

0 Kudos
Reply
3 Replies
1,742 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Zyuan17,

Yes. If you open Doxygen Documentation, if will show you all the APIs.

Doxygen Documentation.png

Doxygen Documentation LPSPI_DRV_SetPcs.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,736 Views
Zyuan17
Contributor III

Zyuan17_0-1666343268137.png

Hi Robin, I still can't find this API in the document and in the component window after I open the Oxygen document.

 

0 Kudos
Reply
1,725 Views
Zyuan17
Contributor III
I have swithed to S32KDS not for Arm, and the problem solved.