I can't find LPSPI_DRV_SetPcs() in the component window

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I can't find LPSPI_DRV_SetPcs() in the component window

跳至解决方案
1,748 次查看
Zyuan17
Contributor III

Zyuan17_0-1666318541267.png

Zyuan17_1-1666318619497.png

 

I am using S32K142EVB to build a project. But there is an API in the example code is not included in the components window.

 

标记 (1)
0 项奖励
回复
1 解答
1,734 次查看
Zyuan17
Contributor III

Zyuan17_0-1666343268137.png

Hi Robin, I still can't find this API in the document and in the component window after I open the Oxygen document.

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,741 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Zyuan17,

Yes. If you open Doxygen Documentation, if will show you all the APIs.

Doxygen Documentation.png

Doxygen Documentation LPSPI_DRV_SetPcs.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,735 次查看
Zyuan17
Contributor III

Zyuan17_0-1666343268137.png

Hi Robin, I still can't find this API in the document and in the component window after I open the Oxygen document.

 

0 项奖励
回复
1,724 次查看
Zyuan17
Contributor III
I have swithed to S32KDS not for Arm, and the problem solved.