How to write the blank "UartFlexioChannelReference" in EB Tresos?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to write the blank "UartFlexioChannelReference" in EB Tresos?

ソリューションへジャンプ
1,140件の閲覧回数
Ashlie
Contributor III

Hello ! I'm new to use EB Tresos. When I try to configure the flexio uart module, I find that I can't understand how to write the blank "UartFlexioChannelReference". What should I write in the blank? So I'm here asking for help.

Thanks.

0 件の賞賛
返信
1 解決策
1,118件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

元の投稿で解決策を見る

2 返答(返信)
1,119件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

1,113件の閲覧回数
Ashlie
Contributor III
Hi Dan,
Thanks for your reply! It really helps a lot. I found that I hadn't configured the channels in Mcl module.
And then, I find I can get the configuration info by Help Contents in EB. Help Contents is very useful for me.
Best wishes,
Ashlie
0 件の賞賛
返信