How to write the blank "UartFlexioChannelReference" in EB Tresos?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to write the blank "UartFlexioChannelReference" in EB Tresos?

Jump to solution
1,139 Views
Ashlie
Contributor III

Hello ! I'm new to use EB Tresos. When I try to configure the flexio uart module, I find that I can't understand how to write the blank "UartFlexioChannelReference". What should I write in the blank? So I'm here asking for help.

Thanks.

0 Kudos
Reply
1 Solution
1,117 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

View solution in original post

2 Replies
1,118 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

1,112 Views
Ashlie
Contributor III
Hi Dan,
Thanks for your reply! It really helps a lot. I found that I hadn't configured the channels in Mcl module.
And then, I find I can get the configuration info by Help Contents in EB. Help Contents is very useful for me.
Best wishes,
Ashlie
0 Kudos
Reply