How to write the blank "UartFlexioChannelReference" in EB Tresos?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to write the blank "UartFlexioChannelReference" in EB Tresos?

跳至解决方案
1,137 次查看
Ashlie
Contributor III

Hello ! I'm new to use EB Tresos. When I try to configure the flexio uart module, I find that I can't understand how to write the blank "UartFlexioChannelReference". What should I write in the blank? So I'm here asking for help.

Thanks.

0 项奖励
回复
1 解答
1,115 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

在原帖中查看解决方案

2 回复数
1,116 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Hi 943552732,

You need to configure FLEXIO_TX and FLEXIO_RX at the "Flexio Logic Channels" in Mcl module.

After that, you can select this "UartFlexioChannelReference" is /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_TX or /Mcl/Mcl/MclConfig/FlexioCommon/FLEXIO_RX

Best regards,

Dan

1,110 次查看
Ashlie
Contributor III
Hi Dan,
Thanks for your reply! It really helps a lot. I found that I hadn't configured the channels in Mcl module.
And then, I find I can get the configuration info by Help Contents in EB. Help Contents is very useful for me.
Best wishes,
Ashlie
0 项奖励
回复