I have too many uart data to receive, and the frame length is not sure, and I do not want so many uart interrupt, so I need timeout receive data+DMA, could NXP give me a demo, thank you very much!
my tool is S32SDK3.0 + S32DS2.2
my tool is S32SDK 3.0 + S32DS2.2
Hello,
There are two available examples which can be useful for you:
After opening S32 Design Studio, go to File -> New S32DS Project From, and there can be found edma_transfer_s32k14x. The purpose of this driver example is to show you how to use the eDMA.
Or you can look at the attached a very simple LPUART TXRX DMA example for the S32K144.
I hope it helps.
Best regards,
Diana