How to use S32K146 UART Idle + DMA Receive Data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use S32K146 UART Idle + DMA Receive Data?

1,352 Views
lzjregister
Contributor I

I have too many uart data to receive, and the frame length is not sure, and I do not want so many uart interrupt, so I need timeout receive data+DMA, could NXP give me a demo, thank you very much!

 

my tool is S32SDK3.0 + S32DS2.2

0 Kudos
2 Replies

1,348 Views
lzjregister
Contributor I

my tool is S32SDK 3.0 + S32DS2.2

0 Kudos

1,326 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

There are two available examples which can be useful for you:

After opening S32 Design Studio, go to File -> New S32DS Project From, and there can be found edma_transfer_s32k14x. The purpose of this driver example is to show you how to use the eDMA. 

Or you can look at the attached a very simple LPUART TXRX DMA example for the S32K144.

 

I hope it helps.

Best regards,

Diana

0 Kudos