Dear sir,
I want to use S32DS command line to import, update code, and cleanbuild.
I can do successfull for the examples(Dio_Example_S32K388) in RTD, but failed for the examples in stacks, like lwip_FreeRTOS_s32k388.
Could you help to check? Or could you provide the method?
I test some examples of S32K388 and S32K344 like below.
Now just lwip_FreeRTOS_s32k388 is failed.
lwip_FreeRTOS_s32k344 is OK.
FreeRTOS_Toggle_Led_Example_S32K388 and FreeRTOS_Toggle_Led_Example_S32K344 are OK.
Dio_Example_S32K388 and Uart_Example_S32K388 are OK.

And my cusomter now is using lwip_FreeRTOS_s32k388, so I need resolve this issue.
Test environment:
S32DS3.6.3
RTD : S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 QLP04
FREERTOS: SW32K3 FreeRTOS 11.1.0 version 6.0.0 Code Drop
TCPIP stack: SW32K3_S32M27X_TCPIP_STACK_3.0.0_D2507
Thanks.
BR,
Sean Wu