How to use CAN RX Filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use CAN RX Filter

2,431 Views
jtpark
Contributor IV

Hello,

I need to use CAN RX Filter as attached.

However, when I checked the exam. code, it was used ID list mode(32 units).

I should use 60 of CAN  ID, ID list was made 32 by example code.

So I want to know how to use CAN RX filter because the application has to use 60 units of ID in CAN network.

Could you let me know how to use CAN RX Filter or example code of Filter?

0 Kudos
Reply
2 Replies

2,035 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I can recommend to either

1. configure the MB to receive all IDs and do SW filtering. You need to clear mask register to receive all IDs

or

2. use the RXFIFO and define desired ID elements in the Filter table. The CAN PAL driver description gives a guide how to use the RXFIFO, see e.g. S32 Design Studio instalation folder .../S32DS/S32SDK_S32K14x_RTM_2.0.0/doc/html/group__can__pal.html

BR, Petr

0 Kudos
Reply

2,035 Views
seop79
Contributor II

Hi.

Please explain each method in detail.

0 Kudos
Reply