How to tell if keys are previously loaded in CSEc?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to tell if keys are previously loaded in CSEc?

848件の閲覧回数
gearhead1107
Contributor IV

I've created a "first boot" routine to initialize the CSEc module on our S32K, but I'd like a way for that routine to see if key slots are currently loaded or not. 

Is there a recommended way to do that, like reading a register?

The only way I can think of based on the documentation is to compute key parameters for a blank key to see if it matches the M4/ M5 from the CSEc module when I try to load a blank key

ラベル(1)
タグ(3)
0 件の賞賛
1 返信

476件の閲覧回数
nevozade
Contributor IV

Hello @gearhead1107 ,

Is there any solution?

0 件の賞賛