How to specify the destination and source addresses for SPI DMA in S32K366 within S32DS 3.6 and RTD5.0?
 VaneB
		
			VaneB
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		To better understand the SPI communication using DMA, an example project named "Spi_Transfer_S32K396" is provided with the RTD 5.0.0 package. This example demonstrates how to configure and use SPI with DMA through the MCAL drivers.
Additionally, you may find it helpful to refer to the following community thread, which includes examples for the S32K344 device. While this is a different MCU from the one you are using, the implementation is quite similar and could serve as a useful reference.
Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500
BR, VaneB