How to solve the ECURset(0x11) error through copy Demo app code into the oneself app?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve the ECURset(0x11) error through copy Demo app code into the oneself app?

918件の閲覧回数
xuruiyi
Contributor I

Hi Tomlin:

     Oneself app add APP_bootloader_exchange_info folder,Please see picture1. Oneself app has the same configuration as demo app of S32K116_17_flash.

    But I don't know why there is an error in the last step after upgrading through ECUBus.

VVBS6 Folder.PNG

VVBS6 FLASH.PNG

VVBS6Boot_ECUBus.PNG

VVBS6Boot.PNG

According to PEAKCAN message information, app doesn't send "02 51 01 00 00 00 00 00" Why ?

 

0 件の賞賛
返信
1 返信

894件の閲覧回数
nxf10035
NXP Employee
NXP Employee

Hi, @xuruiyi 

      For PEAK BUSEAVYY: a Busheavy can occur when you want to send a CAN-message and no other CAN-node is able to send a acknowledge frame (wrong baudrate, CAN-bus not connected, no CAN-termination, a CAN-bus system with only one CAN-node etc.) This is from PEAK. https://forum.peak-system.com/viewtopic.php?t=35

      Suggestion you check APP including APP modules and CAN init status. I think you can integrated a module and test, then you can find which module affect the CAN driver.

BR

Tomlin

0 件の賞賛
返信