Hello Community,
I want to make one GPIO pin (i,e A17) as High and Low. If one condition is true I am making the A17 as High else the A17 is Low.
I configured the clk for A17 with output direction. I tried the PINS_DRV_WritePin(); to make high and PINS_DRV_ClearPins(); for Low and I verified the A17 with multi meter , the output is LOW.
then I tried with the PTA->PSOR |= 1<<17; still the output is Low only it is not changing the state.
can anyone please help me on this.
BR,
Sarwath
解決済! 解決策の投稿を見る。
The Real Time Drivers (RTD) is a collection of user-friendly drivers designed to make the interaction between developers and the different Muc's IPs more dynamic. Is not required but it helps a lot.
You can review more details in: Real-Time Drivers (RTD) | NXP Semiconductors
And yes, the way you are setting the register is also correct.
Best Regards!
Hello @sarwath
You might want to review the example called "Dio_Example_S32K144" from the RTD package.
RTD Download: Real-Time Drivers (RTD) | NXP Semiconductors
Additionally, I believe this topic would be useful to you
HOWTO: Create a Blinking LED example project using... - NXP Community
Hello @JRoberto ,
Why that RTD extension is required.
I found the register to make a pin as HIGH and LOW.
PDDR -- Is the pin used for input or output.
PDOR -- If output, set the value on the pin (0 or 1).
I verified the output, it is changing as per my requirement.
Can you please tell me the above method is correct or not.
BR,
Sarwath
The Real Time Drivers (RTD) is a collection of user-friendly drivers designed to make the interaction between developers and the different Muc's IPs more dynamic. Is not required but it helps a lot.
You can review more details in: Real-Time Drivers (RTD) | NXP Semiconductors
And yes, the way you are setting the register is also correct.
Best Regards!
Thanks for your response @JRoberto. I will dig more about RTC.