How to make FLASH Driver Image file(for S32K344) in Unified bootloader Demo?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to make FLASH Driver Image file(for S32K344) in Unified bootloader Demo?

2,385 次查看
JaydenHsu
Contributor II

Hi Expert:

I referred to the knowledge base post S32K-How to make Flash Driver image. to make Flash Image file for S32K344 but without success
In the knowledge base article, the SDK uses "RTM 4.0.3", Hardware based on S32K142-EVB, but if the SDK is changed to "RTD2.0.0", Hardware based on S32K344-EVB, I would like to know how to use C40_IP to make a Flash driver Image.

BR, Jayden

 

0 项奖励
回复
5 回复数

1,938 次查看
JonAnder_Amante
Contributor I

Hi, I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions. 1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. I need the reply as soon as possible since I have to send a project very soon. 

 

JonAnder_Amante_0-1713768504702.png

 

 

 

 

 

JonAnder_Amante_1-1713768504656.png

 

 

 

 

 

JonAnder_Amante_2-1713768504669.png

 

 

 

 

 

JonAnder_Amante_3-1713768504713.png

 

 

 

 

 

JonAnder_Amante_4-1713768504675.png

 

 

Thank you for all,

0 项奖励
回复

2,363 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@JaydenHsu

Sorry, we don't have a tutorial on how to make a Flash Driver for S32K3.

This article is just for reference. I believe the process of making a Flash Driver is similar, and you need to do it yourself.

(The summary is to store the required functions in the specified memory location, and then directly operate from this location)

 

2,358 次查看
JaydenHsu
Contributor II

Hi Senlent

I have successfully made a Flash Image file, exactly as you said.

Thanks

Jayden

 

 

0 项奖励
回复

1,301 次查看
Voledi
Contributor II

Hi JaydenHsu, 

i have the same case as you when trying to do unified bootloader demo on S32DS 3.6 and RTD5.0.0
I want to change Flash driver to match RTD version 5.0.0 (replace S32K344_FlsDrvRTD100.bin)
Can you show the steps you have done
thanks a lot

0 项奖励
回复

1,241 次查看
raj12
Contributor III
Hello @Voledi,
Please follow this link - https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099 for creation of Flash driver image.
0 项奖励
回复