How to get one project with S2K324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get one project with S2K324

171 Views
IvyGuo
Contributor III

How to get one project rather than a core0 project and core1 the other project,Is there a demo like this? 

0 Kudos
Reply
3 Replies

114 Views
IvyGuo
Contributor III

Sorry, my expression may have caused you misunderstandings; At present, S32K324 has two independent projects based on Core0 and Core1. I would like to confirm if there is a single project with two main functions in it, rather than having the customer maintain two projects.

0 Kudos
Reply

103 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @IvyGuo 

Thank you for the clarification. The RTD versions 2.0.0, 2.0.1, 2.0.2, and 2.0.3 provide an example named "Platform_Multicore_SingleElf_S32K324" which shows the usage of the multicore feature with a single binary file on S32DS for S32K324 derivative.

0 Kudos
Reply

158 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @IvyGuo 

We have available examples of the Inter-Platform Communication Framework (IPCF). Subsystem that enables applications, running on multiple homogenous or heterogenous processing cores, located on the same chip or different chips, running on different operating systems, to communicate over various transport interfaces.

You can download them from S32K3 Standard Software > Automotive SW - S32K3 - Inter-Platform Communication Framework.

 

B.R.

VaneB

0 Kudos
Reply