How to couple a eMIOS PWM signal internally to LCU peripheral ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to couple a eMIOS PWM signal internally to LCU peripheral ?

Jump to solution
479 Views
kyf
Contributor V

Hello there!

I'm was studying the "Lcu_Ip_LcuCOntrolMotor_S32K344" example in order to see how complimentary Outputs are created. I've realized that only the LCU is configured in a way for this to happen.

The PWM signal for this setup is missing and the whole configuration for this to happen.

 

Also reference manual of S32K344 is missing such information.So I would like to ask if someone knows:

1. Is it possible to create complimentary PWM outputs for motor control ? (I believe it is cause of the documentation....)

2. How can I generate 2 complimentary PWM signals from 1 eMIOS timer ? How can I couple/configure the two peripherals ? (I can not find this in the documentation or the config tool)

 

 

I've studied 3-4 times the LCU and eMIOS chapter in the reference manual but still I can not figure this out. If anyone is kind enough to give me a hint or something I would be grateful !

 

0 Kudos
1 Solution
1 Reply
471 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos