How to calculate the usage of STACK by IDE S32DS_ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate the usage of STACK by IDE S32DS_ARM

549 Views
547416104
Contributor III

I  do not know how to calculate the usage of STACK, the IDE is S32DS_ARM. 

547416104_0-1677122170642.png

 

0 Kudos
Reply
1 Reply

525 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @547416104 

well, there's no easy way how to calculate the usage of stack. One option is to use "high water mark" method: generally, you should use a debugger to fill the stack with some pattern (like 0xAA, for example) and then examine all possible operations/paths of your application. Then watch the stack in memory and check the address up to which was the patter rewritten. This should give a good clue what the size of stack should be.

Because the RAM is initialized in startup files in S32DS project due to ECC right after reset (all the RAM is set to "0"), you do not need to bother with filling of some pattern as it is already 0x00.

Another thing is that you can monitor the stack to guarantee that no overflow or underflow happened. This was already discussed:

https://community.nxp.com/t5/S32K/Example-of-DWT-for-stack-usage-monitoring-on-S32K1xx/m-p/1160990

https://community.nxp.com/t5/S32K/Failure-reaction-in-case-of-Stack-overflow-or-underflow-S32K1/m-p/...

https://community.nxp.com/t5/S32K/DWT-on-S32K11x/m-p/960401

Regards,

Lukas

0 Kudos
Reply